cancel
Showing results for 
Search instead for 
Did you mean: 

I want to get information for STM32H7 Series.

JongOk Baek
Associate III
Posted on March 17, 2017 at 02:14

Hello.

I want to know more specification of STM32H7 series.

But, Information was not in ST site.

So I want to get datasheet and reference manual for STM32H7.

If it is possible to share, could you open more information.

I am waiting...

9 REPLIES 9
Nesrine M_O
Lead II
Posted on March 17, 2017 at 11:30

Hi

Baek.JongOk

,

We are glad to see

your interest on the new STM3H7series.

As said during the announcement, the STM32H7 variants will become available along Q2-2

https://community.st.com/0D50X00009XkihHSAR

-Nesrine-

Posted on March 17, 2017 at 12:00

Glimpses of information get available, as STM contributes to the Linux kernel:

- [PATCH 0/5] Add STM32 DMAMUX support

-

https://lkml.org/lkml/2017/3/15/143

Why is general release of chip coupled to release of reference manual?

Posted on March 17, 2017 at 12:20

Why is general release of chip coupled to release of reference manual?

My guess - to keep the Errata documents short ... ;-)

Vladislav Datciy
Associate
Posted on April 25, 2017 at 20:31

Is there any information about the release dates in lqfp208 package?)

Posted on July 08, 2017 at 12:55

Hey there,

Q2 is already gone! Are there any new informations about the release date for the h7?

Greetings!

Posted on July 09, 2017 at 21:46

Q2 is  gone indeed. ST, please update the release info!

AvaTar
Lead
Posted on July 10, 2017 at 08:38

The Keremi newsletter (www<dot>keremi<dot>com) from last states:

STMicroelectronics removed the STM32H753 in the higher temperature grade from the site.

Seems there is still ongoing development and validation ...

Posted on July 15, 2017 at 00:08

Looked at errata, current revision is super buggy. I guess that is the answer why ST basically went silent about it.

In the next revision all of the bugs except one either marked as absent or has workaround. Hope they release it soon.

Posted on July 16, 2017 at 16:57

Dears,

You can check our web site and this new family is at evaluation phase and at production for OEM and few customers, so not yet in full production for all mass market customers. Full validation and qualification of new Technology Flash node of our STM32 MCUs is very important for us and for our customers  {You  ;-) }  as we did in the past to all previous series : 180nm, then 130nm/110nm, then 90nm ( STM32F2/F4/F7 and STM32L4)  and now 40nm  with STM32H7xx. 

Stay Tuned with us, you will release information on our web site, when we are ready !

Cheers,

STOne-32.