cancel
Showing results for 
Search instead for 
Did you mean: 

Any ''Working'' LL Pwm example for Timer 1?

Eric Kelly
Associate
Posted on July 15, 2017 at 20:56

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on July 16, 2017 at 16:17

For TIM1/TIM8 you'd also need to explicitly enable PWM Output. ie MOE bit of BDTR register

/* Enable the Main Ouput */

__HAL_TIM_MOE_ENABLE(htim);
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on July 16, 2017 at 18:15

Thanks!  i'll give that i shot... i see there was a Start PWM i forgot in the HAL above that has it if the timer supports break mode.   seems like 15,16,17 also apply.