2017-09-15 09:55 AM
USI LoRa module
http://www.st.com/en/evaluation-tools/i-nucleo-lrwan1.html
Anyone else ported I-CUBE-LRWAN to the USI Module?
What's your experience with the RSSI level vs other SX1272/SX1276 solutions?
Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-09-29 11:37 AM
I planned to spend one hour to get it work and play with the gateway and server, but after half of a day i got headache, should have bought B-L072Z-LRWAN1.
I-CUBE-LRWAN demo examples does not work without modifications, but cant do a thing when there is no proper documentation for I-NUCLEO-LRWAN1.
There is link to
https://github.com/USILoRaModule/USI_I-NUCLEO-LRWAN1
with some instructions that don't work for me, triedEnd_Node project but got exception inside 'SX1272Init( RadioEvents_t *events )', will check it tomorrow, maybe i will have more luck.
2017-10-01 11:49 AM
I used serial connectivity via LPUART1
2017-10-20 02:13 PM
Ivan Horvat wrote:
there is no proper documentation for I-NUCLEO-LRWAN1.
Indeed.
:(
https://github.com/USILoRaModule/USI_I-NUCLEO-LRWAN1/issues/1
2017-10-20 05:09 PM
I created a pin table, and do actually have the CUBE LRWAN software building for it. You have to wire up the SWD header, and also nuke the firmware because USI has ROP enabled.
The board can then at least be free-standing, but the SX1272 and smaller L0 makes it somewhat less appealing than the Murata. Still enough space to make a Mote using the on-board sensors.
2017-10-20 06:05 PM
Clive One wrote:
I created a pin table,
Any chance of a copy of that, please ... ?
2017-10-20 07:21 PM
Will try pasting it here, hopefully will look a bit better,
/*
USI WM-SG-SM-42
1 GND
2 PA8/RCC_MCO
3 PB10/LPUART_TX
4 PB2/LPTIM1_OUT
5 PA7/ADC_IN7
6 PA1/COMP1_INP ??
7 VREF+
8 GND
9 VDDA
10 PB5/LPTIM1_IN1
11 PA0/SYS_WKUP1
12 GND
13 GND
14 GND
15 GND
16 GND
17 GND
18 GND
19 GND
20 MICRO_RST_N
21 PA9/RF_RST (SX1272)
22 PA2/DIO0 (SX1272)
23 PA3/DIO1 (SX1272)
24 PA5/DIO2 (SX1272)
25 PA6/DIO3 (SX1272)
26 PA10/DIO4 (SX1272) ??TYPO NOT PA1
27 DIO5 (SX1272) ??
28 BOOT0
29 GND
30 VDD_RFS
31 VDD_RFS
32 GND
33 VDD_3V3
34 VDD_3V3
35 GND
36 PB3/SPI1_SCK (SX1272)
37 PB4/SPI1_MISO (SX1272)
38 PA12/SPI_MOSI (SX1272)
39 PA15/SPI1_NSS (SX1272)
40 GND
41 GND
42 GND
43 PB8/RF_SW_CTRL2 TXEN
44 PA4/RF_SW_CTRL1 RXEN
45 GND
46 GND
47 RF_OUT (TEST, HAS U.FL)
48 GND
49 PB7/I2C1_SDA
50 PB6/I2C1_SCL
51 PA13/SWDIO
52 PA14/SWCLK
53 PB1/ADC_IN9
54 PA11/COMP1_OUT
55 PB11/LPUART_RX
56 PB0/ADC_IN8
57 GND
..
81 GND
STM32L052T8Y6 (WLCSP 36)
1 A1 PA13 (SWDIO)
2 A2 PA15 (SPI1_NSS) SX1272
3 A3 PB4 (SPI_MISO) SX1272
4 A4 PB7 (I2C1_SDA)
5 A5 VDD
6 A6 PC14 (OSC32_IN)
7 B1 PA12 (SPI1_MOSI) SX1272
8 B2 PA14 (SWCLK)
9 B3 PB3 (SPI1_SCK) SX1272
10 B4 PB6 (I2C1_SCL)
11 B5 PB8 (RF_SW_CTRL2) TXEN
12 B6 PC15 (OSC32-OUT)
13 C1 PA10 DIO4 SX1272
14 C2 PA11 (COMP1_OUT)
15 C3 PB1 (ADC_IN9)
16 C4 PB5 (LPTIM1_IN1)
17 C5 BOOT0
18 C6 NRST
19 D1 PA9 RF_RST SX1272
20 D2 PB11 (LPUART_RX)
21 D3 PB0 (ADC_IN8)
22 D4 PA0 (SYS_WKUP1)
23 D5 VDDA
24 D6 VSS
25 E1 PA8 (MCO)
26 E2 PB10 (LPUART_TX)
27 E3 PA6 DIO3 SX1272
28 E4 PA4 (RF_SW_CTRL1) RXEN
29 E5 PA2 DIO0 SX1272
30 E6 VREF+
31 F1 VDD
32 F2 PB2 (LPTIM1_OUT)
33 F3 PA7 (ADC_IN7)
34 F4 PA5 DIO2 SX1272
35 F5 PA3 DIO1 SX1272
36 F6 PA1 (COMP1_IN)
*/
Edited 7-Dec-2018 to address forum transition issues, originally posted 21-Oct-2017
2017-10-21 07:29 AM
Great - thanks!
Attached as XLS and tab-separated text files - for anyone else who likes that sort of thing...
________________ Attachments : pin-lst.xls : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyLx&d=%2Fa%2F0X0000000b6T%2Fetfxc.vjxeY3MAf09pF_8Hj3XT7BuCKyjJVIrZt.1Go&asPdf=falsepin-lst.txt.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyLs&d=%2Fa%2F0X0000000b6Q%2F4qE06FGg97RgBWzSFAWIknqNAyye7RAklicMH4hP_tQ&asPdf=false2017-10-21 10:20 AM
The module product page is here:
http://www.usish.com/english/products_WM_SG_SM_42.php
Datasheet:
http://www.usish.com/pdf/WM-SG-SM-42_Product%20SPEC.pdf
There is a link to the ST page for the I-NUCLEO-LRWAN board:
- but no information at all.2017-10-27 08:24 AM
The onboard sensors would be interesting, but I cannot find any documentation ANYWHERE that outlines what sensor is connected how to the USB module (well, the ST source does show how things are connected to the Arduino headers).
Also no description of the SBs and jumpers ...