cancel
Showing results for 
Search instead for 
Did you mean: 

I-NUCLEO-LRWAN1

Posted on September 15, 2017 at 18:55

USI LoRa module

0690X000006045TQAQ.jpg

http://www.st.com/en/evaluation-tools/i-nucleo-lrwan1.html

Anyone else ported I-CUBE-LRWAN to the USI Module?

What's your experience with the RSSI level vs other SX1272/SX1276 solutions?

Note: this post was migrated and contained many threaded conversations, some content may be missing.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
18 REPLIES 18
Ivan Horvat
Associate
Posted on September 29, 2017 at 20:37

I planned to spend one hour to get it work and play with the gateway and server, but after half of a day i got headache, should have bought B-L072Z-LRWAN1.

I-CUBE-LRWAN demo examples does not work without modifications, but cant do a thing when there is no proper documentation for I-NUCLEO-LRWAN1.

There is link to

https://github.com/USILoRaModule/USI_I-NUCLEO-LRWAN1

with some instructions that don't work for me, tried

End_Node project but got exception inside 'SX1272Init( RadioEvents_t *events )', will check it tomorrow, maybe i will have more luck.

Posted on October 01, 2017 at 18:49

I used serial connectivity via LPUART1

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on October 20, 2017 at 21:13

Ivan Horvat wrote:

there is no proper documentation for I-NUCLEO-LRWAN1.

Indeed.

:(

 

https://github.com/USILoRaModule/USI_I-NUCLEO-LRWAN1/issues/1

 
Posted on October 21, 2017 at 00:09

I created a pin table, and do actually have the CUBE LRWAN software building for it. You have to wire up the SWD header, and also nuke the firmware because USI has ROP enabled.

The board can then at least be free-standing, but the SX1272 and smaller L0 makes it somewhat less appealing than the Murata. Still enough space to make a Mote using the on-board sensors.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on October 21, 2017 at 01:05

Clive One wrote:

I created a pin table,

Any chance of a copy of that, please ... ?

Will try pasting it here, hopefully will look a bit better,

/*
 
USI WM-SG-SM-42
 
 1 GND
 2 PA8/RCC_MCO
 3 PB10/LPUART_TX
 4 PB2/LPTIM1_OUT
 5 PA7/ADC_IN7
 6 PA1/COMP1_INP ??
 7 VREF+
 8 GND
 9 VDDA
10 PB5/LPTIM1_IN1
11 PA0/SYS_WKUP1
12 GND
13 GND
14 GND
15 GND
16 GND
17 GND
18 GND
19 GND
20 MICRO_RST_N
21 PA9/RF_RST (SX1272)
22 PA2/DIO0 (SX1272)
23 PA3/DIO1 (SX1272)
24 PA5/DIO2 (SX1272)
25 PA6/DIO3 (SX1272)
26 PA10/DIO4 (SX1272) ??TYPO NOT PA1
27 DIO5 (SX1272) ??
28 BOOT0
29 GND
30 VDD_RFS
31 VDD_RFS
32 GND
33 VDD_3V3
34 VDD_3V3
35 GND
36 PB3/SPI1_SCK (SX1272)
37 PB4/SPI1_MISO (SX1272)
38 PA12/SPI_MOSI (SX1272)
39 PA15/SPI1_NSS (SX1272)
40 GND
41 GND
42 GND
43 PB8/RF_SW_CTRL2 TXEN
44 PA4/RF_SW_CTRL1 RXEN
45 GND
46 GND
47 RF_OUT (TEST, HAS U.FL)
48 GND
49 PB7/I2C1_SDA
50 PB6/I2C1_SCL
51 PA13/SWDIO
52 PA14/SWCLK
53 PB1/ADC_IN9
54 PA11/COMP1_OUT
55 PB11/LPUART_RX
56 PB0/ADC_IN8
57 GND
..
81 GND
 
STM32L052T8Y6 (WLCSP 36)
 
 1 A1 PA13 (SWDIO)
 2 A2 PA15 (SPI1_NSS) SX1272
 3 A3 PB4 (SPI_MISO) SX1272
 4 A4 PB7 (I2C1_SDA)
 5 A5 VDD
 6 A6 PC14 (OSC32_IN)
 7 B1 PA12 (SPI1_MOSI) SX1272
 8 B2 PA14 (SWCLK)
 9 B3 PB3 (SPI1_SCK) SX1272
10 B4 PB6 (I2C1_SCL)
11 B5 PB8 (RF_SW_CTRL2) TXEN
12 B6 PC15 (OSC32-OUT)
13 C1 PA10 DIO4 SX1272
14 C2 PA11 (COMP1_OUT)
15 C3 PB1 (ADC_IN9)
16 C4 PB5 (LPTIM1_IN1)
17 C5 BOOT0
18 C6 NRST
19 D1 PA9 RF_RST SX1272
20 D2 PB11 (LPUART_RX)
21 D3 PB0 (ADC_IN8)
22 D4 PA0 (SYS_WKUP1)
23 D5 VDDA
24 D6 VSS
25 E1 PA8 (MCO)
26 E2 PB10 (LPUART_TX)
27 E3 PA6 DIO3 SX1272
28 E4 PA4 (RF_SW_CTRL1) RXEN
29 E5 PA2 DIO0 SX1272
30 E6 VREF+
31 F1 VDD
32 F2 PB2 (LPTIM1_OUT)
33 F3 PA7 (ADC_IN7)
34 F4 PA5 DIO2 SX1272
35 F5 PA3 DIO1 SX1272
36 F6 PA1 (COMP1_IN)
 
*/

Edited 7-Dec-2018 to address forum transition issues, originally posted 21-Oct-2017

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on October 21, 2017 at 17:20

The module product page is here: 

http://www.usish.com/english/products_WM_SG_SM_42.php

 

Datasheet: 

http://www.usish.com/pdf/WM-SG-SM-42_Product%20SPEC.pdf

 

There is a link to the ST page for the I-NUCLEO-LRWAN board: 

http://www.st.com/en/evaluation-tools/i-nucleo-lrwan1.html

  - but no information at all.
Posted on October 27, 2017 at 15:24

The onboard sensors would be interesting, but I cannot find any documentation ANYWHERE that outlines what sensor is connected how to the USB module (well, the ST source does show how things are connected to the Arduino headers).

Also no description of the SBs and jumpers ...