2023-03-15 08:18 AM
In my code i first setup the sim7600 using blocking mode and later switch to dma. But in blocking mode I'm having trouble receiving data over uart. Using a nucleo it sometimes works very reliably and other times doesn't work at all or it only receives the first letter. on my custom board i once was able to get at ok response but other times it was nothing or some random character. What could be the reason?
2023-03-16 12:50 AM
Post your relevant code
2023-03-16 03:10 AM
sorry, here it is:
that good enough? i can put in the entire code as well if that is better
2023-03-27 03:24 AM
2023-03-27 08:02 AM
There is no way to know what you're doing in SIMTransmitSetup? Post your code as a Code Snippet.
2023-04-06 08:17 AM
it ended up being a poor connection between chip and pcb, thank you for your help