cancel
Showing results for 
Search instead for 
Did you mean: 

I'm trying to interface my STM32F103C6 with ADE7753, So anyone can help me regarding this. I have made the hardware connection correctly but stuck with programming..

DKuma.10
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
DKuma.10
Associate II

I'm not able to establish the communication (unable to read default reg value). Please help me in programming section as soon as possible. 

Don't see any pin connectivity described, ​don't see any software.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
DKuma.10
Associate II

sorry, I didn't get you.

You make several assertions and statements, but provide no actionable detail. Present your problem more effectively.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
DKuma.10
Associate II

You can find my circuit connection attached below.

This code below is just to establish communication between stm32f103c8 and ADE7753 by reading its reg default value in CUBE IDE.

In Clock configuration-36Mhz APB2 peripheral clock.

in SPI-CPOL=high, CPOH=2edge.........Prescaller=64(please describe this)

thank you in advance.

#include "main.h"

#include "spi.h" //SPI1

#include "usart.h" //UART1

#include "gpio.h"

#include <string.h> //using strlen function

void SystemClock_Config(void);

int main(void)

{

void uprintf(char* str) {

HAL_UART_Transmit(&huart1, (uint8_t *) str, strlen(str), 100); //

}

char buffer[32];

uint8_t reg_r=0x00; // 0x00 is for read operation.

uint8_t reg_w=0x80; // For write operation

uint8_t reg = 0x1E; //register address to read its default value.

uint8_t V1; //to store the incomming data from ADE7753

 HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();

 MX_SPI1_Init();

 MX_USART1_UART_Init(); //UART used to transmit data to capture in PUTTY.

 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET); // output low to CS

  HAL_Delay(2); //2 milli second delay.

    HAL_SPI_Transmit(& hspi1,&reg_w,1,1); //set MSB

    HAL_Delay(5); //5milli second delay.

    HAL_SPI_Transmit(& hspi1,&reg,1,1); //reg addr

    HAL_Delay(5); // 5milli second delay

 while (1)

 {

V1= HAL_SPI_Receive(& hspi1,&V1,1,1); //receive data on V1 variable.

    sprintf(buffer, "VRMS:%d\r\n",V1); // for UART data transmit.

  uprintf(buffer);

  HAL_Delay(500);

  HAL_GPIO_TogglePin (GPIOC, GPIO_PIN_13); //led toggle.

  HAL_Delay(100);

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Initializes the CPU, AHB and APB busses clocks 

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

 RCC_OscInitStruct.HSEState = RCC_HSE_ON;

 RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;

 RCC_OscInitStruct.HSIState = RCC_HSI_ON;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

 RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

  Error_Handler();

 }

 /** Initializes the CPU, AHB and APB busses clocks 

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

               |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)

 {

  Error_Handler();

 }

}

void Error_Handler(void)

{

}

#ifdef USE_FULL_ASSERT

void assert_failed(uint8_t *file, uint32_t line)

}

#endif 

DKuma.10
Associate II

i missed 1line of code i.e  

HAL_SPI_Transmit(& hspi1,&reg_r,1,1); //transmit 0x00 for read operation

  HAL_Delay(5); // 5milli second delay

This line of code I wrote just below after sending the address of register.(not in while loop)

DKuma.10
Associate II

@Community member​ waiting for your replay sir.

From my reading of the documentation, you're not sending the register/command properly.

https://www.analog.com/media/en/technical-documentation/data-sheets/ADE7753.pdf

I'd probably start by creating a simple register reading function, and pull out things like the DIEREV and CHECKSUM register, and confirm you can do that properly. Would probably use the chip select more frequently rather that dwell in an infinite loop.

Use a scope or analyzer to look at the signals on the wire, to confirm it matches the diagrams in the manual.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
DKuma.10
Associate II

I read the data sheet before ,but i didn't understand what output i will get in DIEREV and CHECKSUM cause its undefined.

I checked my circuit with SPI connection,its working fine as im getting 2.4V in VREF pin in ADE7753.

I used CRO to check my signals, accept DOUT-MISO singnal, other signals looks fine. I will provide you the MISO output in CRO tommorow.