2019-10-06 3:12 AM
HI Sir.
I will try to work on a project using STM32.
I have a question regarding flash memory usage.
I want to save input data to flash memory but STM flash memory is divided sector.
The capacity of each sector is determined.
ex) STM32F205VE
Sector 0 : 16KB
Sector1 : 16KB
ect..
I have a question here.
For example, when capacity of data to input is 200KB, I will save this data in sector2.
But capacity of sector2 is only 16KB, Is the remaining data automatically saved to the next
sector?
Thank you sir.
Solved! Go to Solution.
2019-10-06 6:25 AM
>>But capacity of sector2 is only 16KB, Is the remaining data automatically saved to the next
The memory blocks are contiguous, You can technically keep writing provided the memory is suitably erased.
If you have a lot of "user" data put it at the end of the array, in the 128KB sectors, away from your code. The erase time for the 128KB sectors is long and may interfere with real-time interfaces.
For small amounts of configuration data (serial number, calibration, etc) make a hole in your firmware(s) so you can use some of the 16KB sectors. The system will need to boot from the first one, although you could fit a loader within 16KB
2019-10-06 6:25 AM
>>But capacity of sector2 is only 16KB, Is the remaining data automatically saved to the next
The memory blocks are contiguous, You can technically keep writing provided the memory is suitably erased.
If you have a lot of "user" data put it at the end of the array, in the 128KB sectors, away from your code. The erase time for the 128KB sectors is long and may interfere with real-time interfaces.
For small amounts of configuration data (serial number, calibration, etc) make a hole in your firmware(s) so you can use some of the 16KB sectors. The system will need to boot from the first one, although you could fit a loader within 16KB
2019-10-06 4:29 PM
Thank you sir
your advice is so helpful to me