cancel
Showing results for 
Search instead for 
Did you mean: 

I had problem about flash memory with STM32H7S78-DK.

jeidi
Associate

Hello.

 

I am using the STM32H7S78-Dk board.
To summarize the problem very simply,
In STM32H7S7L8HXH_flash_default_app.ld, it is set to __FLASH_BEGIN = 0x08000000,
In STM32H7S7L8HXH_RAMxspi1_ROMxspi2_app.ld, it is set to __FLASH_BEGIN = 0x70000000.

In fact, 0x08000000 is not uploaded, and 0x70000000 is uploaded and works.

How can I understand this values?
Can I find it in the parts related to the bootloader in the Datasheet?


Thanks

0 REPLIES 0