cancel
Showing results for 
Search instead for 
Did you mean: 

I can't set adc12 register of STM32G4A1KEU6

BaBQ
Associate
I try to using the bare-metal programming this is my code 

RCC->AHB2ENR |= (1UL<<0);  // Enable clock to GPIO port A
RCC->AHB2ENR |= (1UL<<13); // Enable clock to ADC1,2
 
GPIOA->MODER |= (1UL<<0);  // Set PA0 to analog mode
GPIOA->MODER |= (1UL<<1);
// GPIOA->MODER |= (1UL<<2);  // Set PA1 to analog mode
// GPIOA->MODER |= (1uL<<3);
 
ADC12_COMMON->CCR &= ~(1UL<<0);    // Set ADC1 to independent mode
ADC12_COMMON->CCR &= ~(1UL<<1);
ADC12_COMMON->CCR &= ~(1UL<<2);
ADC12_COMMON->CCR &= ~(1UL<<3);
 
ADC12_COMMON->CCR &= ~(1UL<<18);    // Set ADC1,2 prescaler to 4
ADC12_COMMON->CCR |=  (1UL<<19);
ADC12_COMMON->CCR &= ~(1UL<<20);
ADC12_COMMON->CCR &= ~(1UL<<21);
 
// ADC1->CR |= (1UL<<0); // Enable ADC1
// ADC1->CR |= (1UL<<31);
// ADC1->CR &= ~(1UL<<30); // single-ended input
// ADC1->CR |= (1UL<<2); // Start regular conversion
 
ADC1->CFGR &= ~(1UL<<3); // Set resolution to 12bit
ADC1->CFGR &= ~(1UL<<4);
 
ADC1->CFGR |= (1UL<<12); // Set overwritten with the last conversion result when an overrun is detected
ADC1->CFGR |= (1UL<<13); // Set continue convertion mode
 
ADC1->CFGR  &= ~(1UL<<15); // Set data alignment(right);
ADC1->CFGR2 &= ~(1UL<<0); // Regular Oversampling Disable
 
// ADC1->IER |= (1UL<<2);
 
ADC1->SMPR1 |=  (1UL<<3); // Set sampling time to 247.5 cycle for PA0
ADC1->SMPR1 |=  (1UL<<4);
ADC1->SMPR1 |=  (1UL<<5);
 
ADC1->SMPR1 &= ~(1UL<<6); // Set sampling time to 247.5 cycle for PA1
ADC1->SMPR1 |=  (1UL<<7);
ADC1->SMPR1 |=  (1UL<<8);
 
ADC1->SQR1 |=  (1UL<<0);   // Set channel conversion to 2 channel
ADC1->SQR1 &= ~(1UL<<1);
ADC1->SQR1 &= ~(1UL<<2);
ADC1->SQR1 &= ~(1UL<<3);
 
ADC1->SQR1 &= ~(1UL<<6);   // Set SQ1 for PA0
ADC1->SQR1 &= ~(1UL<<7);
ADC1->SQR1 &= ~(1UL<<8);
ADC1->SQR1 &= ~(1UL<<9);
ADC1->SQR1 &= ~(1UL<<10);
 
ADC1->SQR1 |=  (1UL<<12);  // Set SQ2 for PA1
ADC1->SQR1 &= ~(1UL<<13);
ADC1->SQR1 &= ~(1UL<<14);
ADC1->SQR1 &= ~(1UL<<15);
ADC1->SQR1 &= ~(1UL<<16);
 
ADC1->CR |= (1UL<<0); // Enable ADC1
// ADC1->CR |= (1UL<<31);
ADC1->CR &= ~(1UL<<30); // single-ended input
ADC1->CR |= (1UL<<2); // Start regular conversion

I don't know why it not work, can you help me?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0