2017-07-21 1:46 AM
There is a board programmed with STM32F103 a long time ago.
I can not find the source programmed on the board.So I have to read the data of the mcu, and I wonder if there is any program or method that does the corresponding function.2017-07-21 1:58 AM
Hello!
Try to use
utility.You can read the contents of flash (if not r protected) by SW or JTAG port
2017-07-21 2:10 AM
There is a board programmed with STM32F103 a long time ago.
By a competitor ?
So I have to read the data of the mcu, and I wonder if there is any program or method that does the corresponding function.
If the manufacturer wasn't careless, he had enabled ROP...