2022-02-18 10:30 AM
The timeout of 5 seconds for receiving data from the rtiostream interface has been exceeded. There might be multiple reasons for this failure.
You should:
(a) Check that the target hardware configuration is correct, for example, check that the byte ordering is correct.
(b) Confirm that the target is running.
(c) Consider the possibility of application run-time failures (e.g. divide by zero exceptions, incorrect custom code integration, etc.).
Note (c): To identify possible reasons for the run-time failure, consider using SIL, which supports signal handlers and debugging.
What is the solution for this error
Thank You in advance
If you cannot find a solution, consider using the method setTimeoutRecvSecs of rtw.connectivity.RtIOStreamHostCommunicator to increase the timeout value.