I am reading i2c data from temperature sensor. I need to convert i2c data that I got from sensor to PWM signal. I have generated PWM signal.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-30 1:48 PM
Right now, I am able to get I2C data from sensor. I have generated PWM signal separately with TIM_CH2. But I have no idea how to generate pwm from I2C signal. So, basically I need to control amplitude of pwm from i2c signal. I am using NUCLEO-L011K4 microcontroller development board which is STM32L011K4T6
Here my main part of code:
/* USER CODE BEGIN WHILE */
while (1)
{
uint8_t receiveBuffer[1];
write_register(0x0A, 0X00);
read_register(0X0A, receiveBuffer );
write_register(0X14, 0XC1);
read_register(0X14, receiveBuffer);
HAL_Delay(20);
buffer[0]=0x08;
HAL_I2C_Master_Transmit(&hi2c1,0x50<<1,buffer,1,100);
HAL_Delay(20);
HAL_I2C_Master_Receive(&hi2c1,0x50<<1,buffer,2,100);
// buffer[0] : MSB data
// buffer[1] : LSB data
rawT = buffer[0]<<8 | buffer[1];
Temperature = rawT * 0.005;
HAL_Delay(50);
int32_t counter = 0;
HAL_TIM_Base_Start_IT(&htim2);
HAL_TIM_Base_Start(&htim2);
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_2);
while(counter < 4096)
{
TIM2->CCR2 = counter;
counter += 1;
}
HAL_TIM_PWM_Stop(&htim2, TIM_CHANNEL_2);
HAL_Delay(50);
}
CubeMX selection of pins are attached here.
Thanks
- Labels:
-
I2C
-
STM32L0 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-30 2:17 PM
TIM2->CCR2 would control the PULSE WIDTH, in timer ticks, of the signal.
You'd need to come up with the 0-100% duty as it relates to the temperature range you want to represent, probably with some min/max duty limits.
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
‎2021-08-31 6:30 AM
Thanks for reply. Can you give any example for how to map TIM2->CCR2 to any signal.