cancel
Showing results for 
Search instead for 
Did you mean: 

I am looking for a STM32 MCU with, - Either Two 10-bit ADC with 8 channels each with a sampling rate of 8 MSPS - Or One 12-bit ADC with 8 channels with a sampling rate of 8 MSPS Is there an option to match my requirement? Thanks in Advance.

CManigandan
Associate II
 
4 REPLIES 4
TDK
Guru

Those are beyond the capabilities of the STM32H7 which is the fastest.

https://www.st.com/resource/en/application_note/dm00628458-getting-started-with-the-stm32h7-series-mcu-16bit-adc-stmicroelectronics.pdf

If you feel a post has answered your question, please click "Accept as Solution".
CManigandan
Associate II

Thanks for your response @TDK​ . Much appreciated.

ST Team, any alternate recommendations to meet this requirement with a mix and match of ST components?

MasterT
Lead

If I'm not mistaken, 8 x 8 = 64 MSPS, or mega samples per seconds? Considering constrains of ADC, DMA & uCPU:

H7 limited by ADC - 10.6 MSPS triple interleaved, necessary ~6 pieces;

G4 -//- 20 MSPS 5xADC, 3 pieces.

the best option probably stm32G474. No way to sample continuously, due memory limits

CManigandan
Associate II

@MasterT​  STM32G474 is a good suggestion. Thanks. I am looking it up in detail.