2017-10-23 1:19 PM
Hello,
I want to use the BAM mode, and more specifically, D1/D2 in DSTANDBY, while D3 is in RUN mode. In this mode i want to have ADC3 sampling 3 channels, and transfer the results to RAM using BDMA. From what i can understand i need a LPTIM to trigger the ADC3. I might need a higher sampling rate than the ones LSI/LSE (32k) can provide. I see that i can use HSE through PER_CLK to clock LPTIM.
My question, is it possible to use HSE in BAM mode? The reason i am asking is that there is nothing specific about clock behavior in BAM mode, only in RUN & STOP/STANDBY, and as i understand BAM is in between......
Thanks,
Evgeny
#bam #stm32h7 #adc #dma-adc #adc-trigger #low-power #hseSolved! Go to Solution.
2017-11-29 6:35 AM
Using
a bare metal example from ST that does what is described above, i can see that HSE is still functioning in this mode. This can be concluded from the RM as well, as the HSE is located inside V
DD
domain.2017-11-29 6:35 AM
Using
a bare metal example from ST that does what is described above, i can see that HSE is still functioning in this mode. This can be concluded from the RM as well, as the HSE is located inside V
DD
domain.