2017-04-17 08:08 PM
Thank you for your patronage.
HRTIM does not work. I set up config as shown below.
And, I wrote a program as shown below.
But
HRTIM does not work.
Solved! Go to Solution.
2017-04-18 05:54 AM
Hello
Inoue.Ken
,The functionHAL_HRTIM_WaveformCounterStart should take as parameter a combination of following values:HRTIM_TIMERID_MASTER,HRTIM_TIMERID_TIMER_A,HRTIM_TIMERID_TIMER_B,HRTIM_TIMERID_TIMER_C,HRTIM_TIMERID_TIMER_D,HRTIM_TIMERID_TIMER_E.
Please fix the call of this function in your code then try again.
I recommend you also to have a look to the examples available in the package STM32CubeF3 underSTM32Cube_FW_F3_V1.7.0\Projects\STM32F3348-Discovery\Examples\HRTIM (mainly the exampleHRTIM_BasicPWM).
Also the follwoing application note should bring so much help if you need to explore more HRTIM features:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-04-18 05:54 AM
Hello
Inoue.Ken
,The functionHAL_HRTIM_WaveformCounterStart should take as parameter a combination of following values:HRTIM_TIMERID_MASTER,HRTIM_TIMERID_TIMER_A,HRTIM_TIMERID_TIMER_B,HRTIM_TIMERID_TIMER_C,HRTIM_TIMERID_TIMER_D,HRTIM_TIMERID_TIMER_E.
Please fix the call of this function in your code then try again.
I recommend you also to have a look to the examples available in the package STM32CubeF3 underSTM32Cube_FW_F3_V1.7.0\Projects\STM32F3348-Discovery\Examples\HRTIM (mainly the exampleHRTIM_BasicPWM).
Also the follwoing application note should bring so much help if you need to explore more HRTIM features:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-04-20 03:28 AM
Thank you very much. HRTIM work. If I were thinking by myself, I would not have noticed it. I was indebted to you.