cancel
Showing results for 
Search instead for 
Did you mean: 

HRTIM Alternate function output open drain mode not supported

RexG
Associate III

....so says STM32F334x4/x6/x8 Errata sheet STM32F334x4/x6/x8 Rev Z device limitations

Doc is dated 2021. No answers seen on web.

Has this been fixed yet?

If not, will it be fixed? And if so, when?

Ta lots

Rex

 

 

 

2 REPLIES 2
STTwo-32
ST Employee

Hello @RexG 

unfortunately, there is not any available workaround for now and there is not any potential solution on going. For the typo on table 4 where it is mentioned that there is an existing workaround. It is just a typo on the errata sheet that I've escalated for correction on the coming release (under internal ticket number 196061).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

That's a very simple mask fix!

Badly done ST!