cancel
Showing results for 
Search instead for 
Did you mean: 

How Watch Dog Timer works in STOP mode? STOP mode time is more than 5 min. I want to implement WDT in STOP mode but STOP mode time is more than 5 min and WDT reset time is less than 30 sec.

VChau
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
KnarfB
Super User

The RTC can be used for wake up after an arbitrarily long time.

hth

KnarfB

VChau
Associate II

Thanks for writing, but currently I'm using RTC for wake up....do some take and go back to sleep....

but some time firmware get hang up or stuck some where, So I want to use WDT but i don't know "how

WDT works in Sleep mode"

KnarfB
Super User

The IWDG can continue counting while the MCU is in low power modes or it can pause counting then. So you may set your RTC to wake up say every 4 minutes and the IWDG to 5 minutes. The RTC can then reset the IWDG. What kind of errors do you want the WDG to care for while the MCU is in STOP mode?

hth

KnarfB

Agree, I'm using RTC to Wake up

My question is

What happen if device Hang up (not work properly) in real time scenario(In real application)? How could I reset if device goes Hang up(halt fault)