Question
How to wipe the flash memory of an STM32L476RG
Hi all,
I am working on a research project for my school that involves me programming a microcontroller, however, the program that I most recently flashed to my board causes the processor to quickly heat up and cause a burning smell. I am unsure if the board is damaged yet but I would like to be able to wipe the program without plugging it in so that I can prevent further damage to the board. Is this something that is possible with the STM32L476RG? I am using Keil uVision5 to program my board if that is relevant.