cancel
Showing results for 
Search instead for 
Did you mean: 

How to use Timers ?

Gnahore
Senior

Hi, I'm learning how to use timers by following digikey's tutorial : Getting Started with STM32 and Nucleo Part 6: Timers and Timer Interrupts | Digi-Key Electronics - YouTube

However at 9:41 in the video I don't understand the code : 

// If enough time has passed (1 second), toggle LED and get new timestamp
if (__HAL_TIM_GET_COUNTER(&htim16) - timer_val >= 10000)
{
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
timer_val = __HAL_TIM_GET_COUNTER(&htim16);
}

What does  __HAL_TIM_GET_COUNTER(&htim16) really do? Then what the condition if is testing? 

 

Thanks

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

Wow thank you a lot ! 

Jan presented this:

(uint16_t)(__HAL_TIM_GET_COUNTER(&htim16) - timer_val) >= 10000

You asked to explain this:

(HAL_TIM_GET_COUNTER(&htim16) - timer_val) >= 10000

There is a critically important difference in these lines... Without the cast in front the code is prone to fail at overflow because of integer promotion. In this particular case the only thing that saves the day is the fact that the TIM_CNT register is actually defined as uint32_t for all timers, including the 16-bit ones. But, if both sides of subtraction would be of an uint16_t type, the subtraction would be done as int (signed 32-bit) type, produce a negative result and the comparison would also be done on a signed int type and fail.