2011-12-13 12:24 PM
Hi,
How do I exactly use the fpu after enabled it ? How do I for example put 5.5 into it and add 3.25 for example Dooes my software have to do the conversion and just let the fpu cdo the addition , or is the fpu also capable of doing the conversion from 5.5 integer to float ? Is there any good reference on this subject ? Thanks! Ronny Suy #fpu-vfp2011-12-13 6:26 PM
ARM's documentation might be a good start.
http://infocenter.arm.com/help/topic/com.arm.doc.ddi0439c/DDI0439C_cortex_m4_r0p1_trm.pdf Yes, there are conversion instructions. You should be able to write assembler instructions, if the assembler supports the M4. You should be able to use float/double in C, and use the compiler options to use the intrinsic fpu instructions, instead of using the software floating point library it would utilize for M3 designs.2011-12-14 10:32 AM
2011-12-14 12:00 PM
Ok, well let's try this a different way.
If you want more of a background on floating point, and FPU operations in general, I'd recommend looking at some books/docs on the 80x87 and 68881/68882 type parts. That and the IEEE-754 standard. http://en.wikipedia.org/wiki/IEEE_754-1985 The conversion of floats to/from ASCII-Decimal is a fairly complicated process, and not something implicitly done by the FPU. The FPU can do float-integer conversions, but clearly the range of a 32-bit integer is smaller than a float/double. The ASCII stuff will require that to multiple/divide by 10 and encode/extract the digits. To handle all cases it ends up as a non-trivial exercise. If you have some more constrained numbers, and output format, it can be somewhat simpler. For ASCII to float, look at how this is done with atof() or strtod(), and dtoa() for the double to ASCII http://www.jbox.dk/sanos/source/lib/strtod.c.html http://www.exploringbinary.com/incorrect-directed-conversions-in-david-gays-strtod/ http://opensource.apple.com/source/JavaScriptCore/JavaScriptCore-1C25/kjs/dtoa.cpp Unless you really want to get deep into it, and can do the appropriate testing, I would generally recommend the use of built-in functions, and scanf(), printf(), etc to do conversions. The FPU is designed to do the computational side of the work, the input/output side tends to be more inefficient. http://forums.freescale.com/t5/Kinetis-ARM-Cortex-M4/Using-Cortex-M4-Single-Precision-Floating-point-unit/td-p/741492011-12-15 3:51 AM
Been there, seen it done it!!!
With the EWARM compiler, the normal maths functions, eg sin/exp etc assume long (8byte) reals, even when you have the compiler option 'USE FPU' switched on (theres a dialog for this), there will be no speed up unless you force your reals to be 4 byte by declaring them as float, and if you use trig functions use sinf rather than sin, lastly if you use constants in your expression, force all bits to be 4 byte by using 'float' in the expression, eg with all reals declared as 'float' phinc=(float)0.001*expf(0.001856*adcvalue); and x=sinf(phase); will run fast (approx 28MFlops) but phinc=0.001*exp(0.001856*adcvalue); and x=sin(phase); will run slow, not using the FPU even if enabled!!!!! hope this helps2011-12-15 3:04 PM
How do I for example put 5.5 into it and add 3.25 for example
VLDR.F32 s0,=5.5
VLDR.F32 s1,=3.25
VADD.F32 s3,s0,s1 ; s3 = s0 + s1
VCVT.SF32 s2,s3 ; Convert to integer s2 = (int)s3
VMOV r0,s2 ; Copy to ARM register
2011-12-17 7:35 AM
Dear Clive
Thanks very much for this example ! I tested it , and it really works the result is 8 , so this is correct because of the rounding I guess. If I skip the convert instruction , then the result in S3 = 410C0000 , which is , using a IEEE convertor exactly 8.75 ! For input I think I will use some simple multiply/divide by power of ten and then let the fpu do the job. Example : 17.3845 is the same as 173845 divided by 10000 Moving these to numbers to the fpu can easily be done , and then I let the fpu divide them so the internal result will be 17.3845 At least , I hope so , I will test this very soon ! I you're interested , I will let you know the results Thanks again for your help ! Ronny Suy2011-12-19 2:11 PM
I tested it , and it really works
I do try <G> As Richard points out, the 32-bit float subset supported by the M4 isn't that exciting. Then again the 68882 has 176K transistors, 352 Kflops @ 33 MHz, and had transcendental functions, and 32, 64 and 96-bit floats.2011-12-20 2:19 PM
2012-07-13 3:01 AM
I am using C in Keil here, for the STM32F4 Discovery, with FPU being used.
My problem is attempting to assign a signed int or constant to a Float variable always resulted in the Float being 0. I recast the int or constant as (float) on the righthand side.int16_t myInt=0x12345;float myFloat;myFloat=(float)myInt; //gets zeroIs this just a Keil problem, or do I need to be handling floats ''differently'' somehow?