2018-09-08 12:24 AM
Dear All
Nice to meet you.
At First My english is poor. Please understand me.
I want use M95512 (EEPROM) with STM32F103RCT6 SPI3
but now I check Oscilloscope SCK, MOSI, MISO. Only work MOSI have signal
now no work SCK.... How to Init. SPI3
Please check my code.
Thank you ^.^
void SPI3_Config(void){
SPI_InitTypeDef SPI_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
SPI_Cmd(SPI3, DISABLE);
GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE);
GPIO_PinRemapConfig(GPIO_Remap_SPI3, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE);
// SCK MOSI
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_5;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_Init(GPIOB, &GPIO_InitStructure);
// MISO
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOB, &GPIO_InitStructure);
// Configure CS pin as output floating
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
// SPI configuration -------------------------------------------------------
SPI_I2S_DeInit(SPI3);
SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_8;
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_Init(SPI3, &SPI_InitStructure);
SPI_Cmd(SPI3, ENABLE);
SPI_SSOutputCmd(SPI3,DISABLE);
SPI_I2S_ITConfig(SPI3,SPI_I2S_IT_RXNE,ENABLE);
}
2018-09-08 1:45 AM
GPIO_PinRemapConfig(GPIO_Remap_SPI3, ENABLE);
I don't use 'F1, but looking into RM0008 it appears that SPI3_SCK is at PB3 when SPI3 is *not* remapped.
2018-09-08 3:12 AM
Thank you ~ ^.^ waclawek.jan
I was use like this. but work same (no SCK)
GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE);
// GPIO_PinRemapConfig(GPIO_Remap_SPI3, ENABLE);
I was use like this. but also work same (no SCK)
// GPIO_PinRemapConfig(GPIO_Remap_SWJ_JTAGDisable, ENABLE);
// GPIO_PinRemapConfig(GPIO_Remap_SPI3, ENABLE);
When I use SPI1 with M95512(EEPROM) than ... It's work...
But..... change SPI3..... no work...
Please check it.
2018-09-08 4:16 AM
Now Can Work~....
I change position. end of GPIO Init