2017-05-09 10:09 PM
2017-05-10 01:39 AM
Hi
raja.immanuel
,I recommend you to start from ready example under the STM32F4 cube firmware package,
STM32Cube_FW_F4_V1.0\Projects\STM324x9I_EVAL\Examples\FMC\FMC_SDRAM_DataMemory
The example scenario provides the procedure to follow to use the external SDRAM as data memory.
-Nesrine-
2017-05-10 01:50 AM
I hope you verified you don't try to access the SDRAM before initializing it.
And have you checked / debugged that the SDRAM access works at all, at the assumed addresses ?
2017-05-10 04:04 AM
Dear Avatar,
I have tried as per the STM32Cube_FW_F4_V1.0\Projects\STM324x9I_EVAL\Examples\FMC\FMC_SDRAM_DataMemory
I have replaced the same startup file and system_stm32fxxx.c and changed compiler settings as per that exaple.Eventhough the issue persist.
Regards,
Immanuel Raja
________________ Attachments : 84C10FE7E3FD49D2A0A577B5B549760E.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyg2&d=%2Fa%2F0X0000000bAn%2FF16BmTHlv0ioN9Modgkxk1EiWbaxyxyVy1Bygr7hhW0&asPdf=false