2017-01-19 05:32 AM
Hi, I have a problem with low power mode. I want to use the watchdog with the stm32l0xx.
But when I go in stop mode, I can not disable or frooze the watchdog counter (only possible with l4 family).
And in a perfect world I don't want to wake up the stm in order to refresh the watchdog. It's not very efficient for power saving.
Is there a solution ?
Tanks.
David.
#low-power-mode #stop-mode #stm32l0 #iwdg2017-05-30 03:29 PM
I know this is an old question but the answer is... you cant!
From reference manual:
20.3.4 Behavior in Stop and Standby modes Once running, the IWDG cannot be stopped.