cancel
Showing results for 
Search instead for 
Did you mean: 

How to start with Discovery

gsantha
Associate II
Posted on September 13, 2011 at 00:06

Hi!

I've just purchased my board and I'd like to create my own applications. Is there any example code or similar to get me started? I checked the demo code which is very complex and also found a peripherial library with template project but that is not for Discovery. How can I start with this board?

Any idea would be great,

Regards, Greg73
12 REPLIES 12
Posted on October 01, 2011 at 23:38

Blog about the Discovery Board:

http://gostm32.blogspot.com/

kohchengsing
Associate II
Posted on October 12, 2011 at 03:02

Perhaps you can find some simpler examples here: 

http://singamicro-63-stm32l152-k1.blogspot.com/

Actually, the STM32VL-Discovery board with the STM32F100 may be easier.

gsantha
Associate II
Posted on November 27, 2011 at 19:42

All right, I eventually fitted the peripherial library to my board and now I'm kind of happy with it. It wasn't so bad indeed but required more work than I expected. Anyway, all is well that ends well. :)