2019-03-21 5:36 AM
I am trying to connect the VL53L1X distance sensor to a B-L072z-lrwan dicoboard so it can send data using the lorawan stack .
This is my first project using a hal and i cant get the I2C connection working.
The output to my serial monitor is: 536872016,status
My code right now:
GPIO init
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOB_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_I2C1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_I2C1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
}I2C init:
static void MX_I2C1_Init(void)
{
hi2c1.Instance = I2C1;
hi2c1.Init.Timing = 0x00300F38;
hi2c1.Init.OwnAddress1 = 164;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
}ranging function
void AutonomousLowPowerRangingTest(void)
{
static VL53L1_RangingMeasurementData_t RangingData;
//PRINTF("Autonomous Ranging Test\n");
status = VL53L1_WaitMeasurementDataReady(Dev);
if(!status)
{
status = VL53L1_GetRangingMeasurementData(Dev, &RangingData);
//status =0;
PRINTF("%d,status\n");
if(status==0){
PRINTF("%d,%d,%.2f,%.2f\n", RangingData.RangeStatus,RangingData.RangeMilliMeter,
(RangingData.SignalRateRtnMegaCps/65536.0),RangingData.AmbientRateRtnMegaCps/65336.0);
}
status = VL53L1_ClearInterruptAndStartMeasurement(Dev);
}
// return status;
}Main:
int main( void )
{
/* STM32 HAL library initialization*/
HAL_Init();
/* Configure the system clock*/
SystemClock_Config();
/* Configure the debug mode*/
DBG_Init();
/* Configure the hardware*/
HW_Init();
/* USER CODE BEGIN 1 */
// initialize vl53l1x communication parameters
MX_GPIO_Init();
MX_I2C1_Init();
HAL_I2C_Init(&hi2c1);
HAL_I2C_MspInit(&hi2c1);
dev.I2cHandle = &hi2c1;
dev.I2cDevAddr = 0x52;
/*** VL53L1X Initialization ***/
VL53L1_WaitDeviceBooted(Dev);
VL53L1_DataInit(Dev);
VL53L1_StaticInit(Dev);
VL53L1_SetDistanceMode(Dev, VL53L1_DISTANCEMODE_MEDIUM);
VL53L1_SetMeasurementTimingBudgetMicroSeconds(Dev, 50000);
VL53L1_SetInterMeasurementPeriodMilliSeconds(Dev, 500);
VL53L1_StartMeasurement(Dev);
/* USER CODE END 1 */
/*Disbale Stand-by mode*/
LPM_SetOffMode(LPM_APPLI_Id , LPM_Disable );
PRINTF("VERSION: %X\n\r", VERSION);
/* Configure the Lora Stack*/
LORA_Init( &LoRaMainCallbacks, &LoRaParamInit);
LORA_Join();
LoraStartTx( TX_ON_TIMER) ;
SetPWR(Sensor, PWR_ON);
while( 1 )
{
if (AppProcessRequest==LORA_SET)
{
/*reset notification flag*/
AppProcessRequest=LORA_RESET;
/*Send*/
Send( NULL );
}
if (LoraMacProcessRequest==LORA_SET)
{
/*reset notification flag*/
LoraMacProcessRequest=LORA_RESET;
LoRaMacProcess( );
}
/*If a flag is set at this point, mcu must not enter low power and must loop*/
DISABLE_IRQ( );
/* if an interrupt has occurred after DISABLE_IRQ, it is kept pending
* and cortex will not enter low power anyway */
if ((LoraMacProcessRequest!=LORA_SET) && (AppProcessRequest!=LORA_SET))
{
#ifndef LOW_POWER_DISABLE
LPM_EnterLowPower( );
#endif
}
ENABLE_IRQ();
/* USER CODE BEGIN 2 */
AutonomousLowPowerRangingTest();
/* USER CODE END 2 */
}
}
2019-03-21 6:41 AM
After measuring the SCL and SDA on an osiloscope i found out that they are both set to 1.