2022-10-01 7:05 AM
I try to write the driver for I2C and I open the reference I face a problem in setting values for SCLDEL SDADEL SCLH SCLL and I don't know how to set theses values. I kept searching and I saw there is an Excel sheet you can enter the Pclk and I2C speed frequent,rise time ,fall time, and choose filters then you will get the value I try to apply the example which is provided in the below picture but the result is not the same as the photo
So to summarize What do I need to help me in it?
Why the result is different?
How to set values of ( SCLDEL SDADEL SCLH SCLL )? It will be great if you give a formula to understand instead of reference which I can't understand it.
Solved! Go to Solution.
2022-10-26 2:30 AM
Hello @AOmar.2 and welcome to the Community :D
I suggest you look to the Reference manual (RM0316) in Sections for more details:
STM32F303xB/C/D/E, STM32F303x6/8, STM32F328x8, STM32F358xC, STM32F398xE advanced ARM®-based MCUs
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-10-26 2:30 AM
Hello @AOmar.2 and welcome to the Community :D
I suggest you look to the Reference manual (RM0316) in Sections for more details:
STM32F303xB/C/D/E, STM32F303x6/8, STM32F328x8, STM32F358xC, STM32F398xE advanced ARM®-based MCUs
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.