2022-03-11 7:01 PM
I want to read and write application code with comments in STM32 MCU flash or external memory.
When I read flash from STM32 MCU I want comments also present there in code.
How can I do this? It is possible with MCUs inbuilt memory or need external memory?
2022-03-11 8:35 PM
>>It is possible with MCUs inbuilt memory or need external memory?
Wouldn't that really depend on how much space your "code + comments" consume.
Is this some interpreted source code?
2022-03-11 8:44 PM
we can assume (code + comments ) > MCU flash size then how it is possible?
2022-03-11 9:42 PM
ST has parts with 2MB of internal flash.
Most could take external SPI, and QuadSPI NOR Flash, so 16MB up 128MB readily available.
For GB look to SD cards or eMMC chips using NAND Flash.
2022-03-12 4:40 PM
What is the compiler settings for this so it's donot remove comments?
Is there any example project of external QSPI memory interface with STM32?