‎2019-03-30 03:42 PM
I am using the STM32F103C8 (blue Pill) and have been having lots of troubles with reading multiple channels on ADC1. Here is my init code using firmware 1.7:
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/**Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 4;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_2;
sConfig.Rank = ADC_REGULAR_RANK_3;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/**Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_3;
sConfig.Rank = ADC_REGULAR_RANK_4;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
I am trying to read from analog pins PA0-3, and I am getting very odd results. Whenever I try change the value of just one ADC Pin, all of the values seem to change, and then on some pins when I change the value I see no response from the STM at all. Anyone have similar problems or see something up with my init? Here is how i call for values:
HAL_ADC_Start(&hadc1);
if(HAL_ADC_PollForConversion(&hadc1, 100) == HAL_OK);
adc0 = HAL_ADC_GetValue(&hadc1);
if(HAL_ADC_PollForConversion(&hadc1, 100) == HAL_OK)
adc1 = HAL_ADC_GetValue(&hadc1);
if(HAL_ADC_PollForConversion(&hadc1, 100) == HAL_OK);
adc2 = HAL_ADC_GetValue(&hadc1);
if(HAL_ADC_PollForConversion(&hadc1, 100) == HAL_OK);
adc3 = HAL_ADC_GetValue(&hadc1);
HAL_ADC_Stop(&hadc1);
‎2019-03-30 09:26 PM
I know it will be little consolation, I tried multi-channel polling and gave up. I switched to DMA and getting pretty consistent results.
‎2019-03-31 03:53 AM
Well I program at a lower level but simply trigger the ADC on each channel in turn in my code and it works fine with little crosstalk
void start_ADC(uint8_t ADC_type) // start A-D convertors
{
ADC0_MUXPOS = ADC_type;
ADC0_COMMAND = 0b00000001;
}
if (ADC0_INTFLAGS & 1) // should be ready - conversion takes 8.7uS
Vadc1 = ADC0_RES;
‎2019-03-31 07:51 AM
Soon as my two projects are done, going to get learning LL and register on the STM32L4 processors. Horrible HAL is too goofy :dizzy_face:
‎2019-03-31 08:00 AM
I tried it when it first came out and had to stop as too many problems. I keep telling myself I'll give it another try sometime but still haven't umpteen years later :)
‎2019-03-31 08:10 AM
You need to use DMA to read from multiple channels. Otherwise the ADC will only read from the channel on rank 1.