Skip to main content
CH_bot_
Associate II
July 14, 2021
Question

How to read continuous data from an external ADC via the SPI interface with DMA?

  • July 14, 2021
  • 10 replies
  • 6472 views

I am not sure how to read continuous data from an external ADC. The ADC has an SPI interface and a data ready pin.

Every time the data is ready, the data ready pin goes low and the data can be read. 

My goal is to read out the data via the DMA every time the data ready pin goes low.

Is this possible?

Unfortunately I have not found any examples.

I would be very grateful for any help.

    This topic has been closed for replies.

    10 replies

    David Littell
    Senior II
    July 14, 2021

    Use the ADC's data ready pin transition low to create an interrupt. In the interrupt handler do the SPI DMA call.

    CH_bot_
    CH_bot_Author
    Associate II
    July 15, 2021

    Thank you very much for this advice. 

    This helps in the beginning to increase the performance

    waclawek.jan
    Super User
    July 14, 2021

    Which STM32?

    There may be ways to automate this without need for interrupt - in models with DMAMUX, using that; in models without, e.g. by generating SPI clocks/framing using cascaded timers triggered by the external signal. Just read the Reference Manual, and write many many small and simple experiments.

    JW

    CH_bot_
    CH_bot_Author
    Associate II
    July 15, 2021

    Thank you very much for your advice.  

    It would be really nice to do this without interrupts. 

    I am using the STM32F303K8, so I have to use cascaded timers in this case.

    Unfortunately I am not sure how to do this.

    Is it possible to trigger the timer with the Data Ready pin and this calls the DMA request for the SPI interface?

    MasterT
    Lead II
    July 15, 2021
    1. Two timers, one generates for CS, another (gated mode driven by CS event) - SPI clock.
    2. I2S, PCM mode. Provide higher frequency (PWM) clock to ADC that is synchronous to I2S frame rate, than you don't need to read DR pin.
    3. stm32H7 has NSSP - nice feature I discovered recently. Pity other stm32 uCPU product lines doesn't have.
    Explorer II
    August 28, 2023

    I know it was a long time ago since you did answer this but how can the NSSP help us extract data from an external ADC via the SPI interface with DMA?

    MasterT
    Lead II
    August 28, 2023

     The idea is to read external adc w/o GPIO interrupt, so sampling rate is not restricted by interrupt latency, 1usec or so on 480 MHz uCPU , or less than 1 MSPS.

    Knowing number of  clock cycles for adc to complete conversion, it's not required to read DRDY. Especialy, when some ADC (AD798x etc) runs at 1.33 MSPS and doesn't have DRDY pin  at all.

    1. Provide master clock from stm32H7 to adc, so adc running in sync.

    2. Set up SPI-DMA in continuous mode, than adjusting NSSP delay time make SPI to run in sync with ADC conversion complete frequency.

      Changing prescaller of the SPI clock divider if NSSP delay time reach a limit.

    Succsessfuly tested on stm32H743zi2 interfaced to MCP3562 & MAX11270, plan for ads127l11 and what ever comes after > 1MSPS 24-32 bits. 

    waclawek.jan
    Super User
    July 15, 2021

    > Is it possible to trigger the timer with the Data Ready pin and this calls the DMA request for the SPI interface?

    Yes, that's an option too. Just set the given TIM channel to Input Capture and trigger DMA from it, transferring from memory to SPI's data register.

    As I've said, read all related chapters in RM and experiment, while observing all the relevant pins using a logic analyzer.

    JW

    waclawek.jan
    Super User
    August 28, 2023

    Just to avoid any confusion: there is no mention of NSSP in the 'H7 RM.

    NSSP in SPI of newer models other than 'H7 (e.g. the 'F3 as the OP uses) inserts a pulse on NSS with duration of exactly 1 SCK; and that is not very helpful here.

    What I suspect @MasterT is referring to above, is the feature which inserts a delay between frames using the MIDI bitfield, which allows to fine-tune duration of one frame (or a sequence of frames) - in this case, adjusting it to the total sampling cycle of the ADC. A pulse simlar to NSSP can be optionally output to NSS (by setting SSOM bit, if the delay provided by MIDI is long enough), but that is not important for this purpose.

    JW

    MasterT
    Lead II
    August 28, 2023

    Correct. Likely I just catch term (not existed at that time officially) from

     hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
     hspi2.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;

    NSSP...Mode

    Advantage of using this mode is to get complete flexibility over sampling rate, SPI in this case running from PLL3.

    There is poor alternative, to use Timer->DMA->SPI link, that provides only rough approximation to desired frequency (integer dividers of the main 480 MHz) and may not be acceptable for audio. Secondly, I'm not sure if SPI driven by DMA generates NSS (Chip Select or  Bus select - frame marking SPI bus in essence) .

    I had a hard time to figure out all bugs regarding CS pin in different F4/F7/H7 products and in different modes of operation : TI / Motorola / Master-slave etc, so was very happy to discover that two lines of code takes all my headache away