2020-12-23 10:10 AM
2020-12-23 11:05 AM
Plenty of information about this in the user manual. Look at "6.2.2 Supplying the board from VIN: 7 V to 12 V/800 mA".
2020-12-24 01:34 AM
I have a 1000mA 5V Power-supply with micro-USB connector.
I want to plug this into the USB-OTG on the 735 an set the power-jumper to USB-OTG. The st-link v3 I connect to its connector on the 735.
Okay?
2020-12-24 07:22 AM
I'm fairly certain the user manual says you can only draw 500mA from the USB connector.
2020-12-25 05:47 AM
The STM32H735G-DK BOARD seamed to be debree now. It is unbeleaveable that the board will have to be powered by the arduino 5V female connector. How can it stand then on its 4 feed? I hope Digikey will take it back.