2025-03-03 12:38 AM
I was trying to interface W25Q256 with STM32H563ZI in QuadSPI mode as i have done with normal SPI it was working fine as i need to operate at higher frequency than normal spi for continous read and write operation. I tried to read Device information first but i was unable to read the device information mode.
This is the parameter that i have set.
Also i have attached the programming file.
I need help in debugging the code and configuring the parameter in stm32cube ide if needed.
2025-03-03 4:09 AM - edited 2025-03-03 4:13 AM
Hello @Shubham08,
Is the Quad mode enabled on both sides in order to communicate properly
- QUADSPI side
- Quad-spi memory side.
I recommend you to look at AN5050 Table 8 and check your OCTOSPI configuration.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-03 8:35 AM
Sir i will follow the document and get back if any problm occurs