2020-08-18 5:54 AM
Hello,
The system has a MCU STM32L151 and here the details.
ESD testing + / - 15 KV contact on the box enclosure. PCB is inside and the ground frame is connected to the board and box.
F/W Test:
I performed ESD test in STOP mode only. The lock is always in sleep when I zap the box.
I noticed interesting behavior.
Here are my notes:
To solidify the firmware, we need to understand each problem independently and see the best thing to do. And now, I am confused! I am not sure to apply a solution in PVD could fix it.
It's possible to change the hardware or mechanical stuff. But, I would like to see if you can improve the firmware to prevent any problem also.
Any ideas?
Thanks
Christian
2020-08-18 10:12 AM
up
2020-08-18 2:13 PM
The chip is not safe to 15 kV by itself. If you need that level of protection, you will need to add external ESD protection chips.
ESD is not a problem you can solve in firmware. It is a hardware issue.
2020-08-19 5:38 AM
My last tests were done at 15 KV but I already got issues at +/- 8 KV. The same symptoms occurred at +/- 15 KV and faster!
2020-08-19 6:29 AM
Why are you expecting a chip that is rated to 2kV to survive a 15kV shock?