cancel
Showing results for 
Search instead for 
Did you mean: 

How to implement a few cycles delay macro or function

CTabo.1
Senior

Hello,
I need to implement delay macro, lasting just a few cycles.

As the delay is so small I would not like to use TIMs o DWT.

On Texas Instruments DSPs, I was used to implement this nanoseconds delays, using NOP() instructions.
Unfortunately, as also written in STM32 Programming Manual this is not a good pattern on Cortex processors.

On a previous post, related to another issue, I was suggested to use Data Memory Barrier (DMB), Data Synchronization Barrier (DSB), and Instruction Synchronization Barrier (ISB) instructions, instead of NOPs.

How can I use this instructions, to implement a few cycles delay macro?

Regards,
Carlo

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12

@CTabo.1 wrote:

it may be necessary to encapsulate the two consecutive readings instructions between #pragma directives to disable any optimizations.

 


Possibly, although I'd have thought that the RHS should be qualified as volatile - so might not get optimised?

Maybe alternative to make sts volatile?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

> However it may be necessary to encapsulate the two consecutive readings instructions between #pragma directives to disable any optimizations.

Registers are marked as volatile. The compiler must read them on every access in your program.

If you feel a post has answered your question, please click "Accept as Solution".

@TDK , @Andrew Neil 

Yes, you guys are both right.
The registers are markerd as volatile, so eventual optimizations should not create problems.

Thank you very much,
Carlo