2023-12-12 8:58 AM - edited 2023-12-12 9:34 AM
Hi
I am using the USB CDC on a STM32L433 with the command MX_USB_DEVICE_Init(); to communicate through the USB. In my app, I go into standby mode (by using the HAL_PWR_EnterSTANDBYMode()) command. How do I disable the USB before entering standby? I tried the the command USBD_DeInit(&hUsbDeviceFS) , but got a hardware fault. Anyone let me know the best way to disable it?
Best Regards
Scott
Solved! Go to Solution.
2023-12-12 9:43 AM
Hello @SSmit.13
I suggest you set the USBFSRST High then Low to reset the USB FS and set the USBFSEN Low to disable the USB FS clock.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-12 9:43 AM
Hello @SSmit.13
I suggest you set the USBFSRST High then Low to reset the USB FS and set the USBFSEN Low to disable the USB FS clock.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-14 1:17 PM
That worked, many thanks
Scott