2012-10-16 9:50 AM
hello forum,
the processor is STM32F103
I have an H bridge for DC motor
I want complementary outputs of CH1 and CH1N
I setup the timer 1 as following
TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = 7200; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; TIM_OCInitStructure.TIM_Pulse = 2000; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCNIdleState_Set;TIM_OC1Init(TIM1, &TIM_OCInitStructure);
TIM_OC2Init(TIM1, &TIM_OCInitStructure); TIM_BDTRInitStructure.TIM_OSSRState = TIM_OSSRState_Enable; TIM_BDTRInitStructure.TIM_OSSIState = TIM_OSSIState_Enable; TIM_BDTRInitStructure.TIM_LOCKLevel = TIM_LOCKLevel_OFF; TIM_BDTRInitStructure.TIM_DeadTime = 0xCA; TIM_BDTRInitStructure.TIM_Break = TIM_Break_Disable; TIM_BDTRInitStructure.TIM_BreakPolarity = TIM_BreakPolarity_Low; TIM_BDTRInitStructure.TIM_AutomaticOutput = TIM_AutomaticOutput_Disable;TIM_BDTRConfig(TIM1, &TIM_BDTRInitStructure);
then I call below functions to start PWM
however I cant get complemantary output at CH1 and CH1N
I get the same polarity of both CH1 and CH1N ( CH1N is the same as CH1 )
how can I get complementary outputs ?
thank you TIM_SelectOCxM(TIM1, TIM_Channel_1, TIM_OCMode_PWM1); TIM_CCxCmd(TIM1, TIM_Channel_1, TIM_CCx_Enable); TIM_CCxNCmd(TIM1, TIM_Channel_1, TIM_CCxN_Enable); TIM_SelectOCxM(TIM1, TIM_Channel_2, TIM_ForcedAction_Active); TIM_CCxCmd(TIM1, TIM_Channel_2, TIM_CCx_Disable); TIM_CCxNCmd(TIM1, TIM_Channel_2, TIM_CCxN_Enable); #tim-stepper-h-bridge #timer-dead-time #timer-complementary-outputs
2012-10-16 10:15 AM
7200-1 surely?
This is how ST does it in their examples/* Channel 1, 2 and 3 Configuration in PWM mode */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable;
TIM_OCInitStructure.TIM_Pulse = Channel1Pulse;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;
TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low;
TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set;
TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset;
TIM_OC1Init(TIM1, &TIM_OCInitStructure);
TIM_OCInitStructure.TIM_Pulse = Channel2Pulse;
TIM_OC2Init(TIM1, &TIM_OCInitStructure);
TIM_OCInitStructure.TIM_Pulse = Channel3Pulse;
TIM_OC3Init(TIM1, &TIM_OCInitStructure);
2012-10-17 1:08 PM
I changed the initializing code according to your example
and I call folowing functions to start PWM
TIM_SelectOCxM(TIM1, TIM_Channel_1, TIM_OCMode_PWM2); TIM_CCxCmd(TIM1, TIM_Channel_1, TIM_CCx_Enable); TIM_CCxNCmd(TIM1, TIM_Channel_1, TIM_CCxN_Enable);yes I got complementary signals at CH1 and CH1N
however dead time generator insert dead time at wrong places
I draw the osciloscope image above
as you can see ON times of mosfets collide ( the dark lines )
I want dead times like as shown in the dashed lines
what I must change in the code ?
2012-10-17 1:52 PM
PWM motor control isn't my thing, but perhaps
TIM_BDTRInitStructure.TIM_LOCKLevel = TIM_LOCKLevel_1;2012-10-18 6:54 AM
Because you have OCxN active low the dead time won't work. During the deadtime gap both signals are driven to the inactive level....low for OCx and high for OCxN, so the H-Bridge stays on. OCx and OCxN polarity should match when driving a bridge, unless you have an inverter on one side.
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low; should be: TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_High; Jack Peacock