cancel
Showing results for 
Search instead for 
Did you mean: 

How to get 2 Mbytes RAM with STM32F407/427 and IS61WV102416 memory?

Yurii Stukalo
Associate II
Posted on June 12, 2018 at 14:47

How to get 2 Mbytes RAM with STM32F407/427? I have Dev. Kit  STM3240G-EVAL wich have STM32F407IGH MCU and  IS61WV102416BLL-10MLI 16 Mbit (1Mx16) SRAM memory on the board. One example which provide ST for the dev. borad I have 1 Mbytes external SRAM (linker regions for RAM is Start: 0x64000000 End: 0x640FFFFF). How can I get 2 Mbytes RAM with the memory? Or it is not possible with the memory as it have 1Mx16 configuration ?  Thanks.

#fmc #sram
4 REPLIES 4
Tomas DRESLER
Senior II
Posted on June 12, 2018 at 15:01

The function BSP_SRAM_Init shall give you the whole 2MB space. You can try to modify the linker script to address whole 0x200000 space on top of 

0x64000000 SRAM start address.

Give it a try, don't take all examples as granted bug-free :-)

Posted on June 12, 2018 at 15:22

If you configure the memory/pins properly, and watch the jumpers (trace), you should be able access all 2MB

0x64000000- 0x641FFFFF

The address bits A0-A20 on the device represent A1-A21 in STM32 address space, and the byte lanes are managed on the D0-D7,D8-D15 level along with BLE,BHE

IS61WV102416BLL-10MLI 1Mx16 (2MB)

CY7C1071DV33-12BAXI  2Mx16 (4MB)

These look to define the memory at 2MB in size

STM32Cube_FW_F4_V1.21.0\Drivers\BSP\STM324xG_EVAL\stm324xg_eval_sram.c

STM32Cube_FW_F4_V1.21.0\Drivers\BSP\STM324xG_EVAL\stm324xg_eval_sram.h

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on June 12, 2018 at 15:25

The BSP examples look to be Ok, the bus wiring uses a NC pin on the 2MB chip, and there is an alternate 4MB chip option.

The high order address bits are used by the TRACE functionality, so if using a trace pod you need to use less external memory (512KB?)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Yurii Stukalo
Associate II
Posted on June 12, 2018 at 17:32

After changing linker it working, thanks both for help.