2023-11-02 07:35 AM - last edited on 2023-11-08 01:01 AM by Amel NASRI
2023-11-02 07:44 AM
It is STM32F103C8T6 blue pill. This board is supported by Arduino IDE.
2023-11-02 07:44 AM
It is STM32F103C8T6 blue pill. This board is supported by Arduino IDE.
2023-11-02 07:47 AM
Or it could be a fake.
You'd try connecting with an ST-LINK via the SWDIO, SWCLK, NRST, VCC, GND, etc
With BOOT0=HIGH the USB connector might present as "STM32 BOOT DEVICE" or similar, and you can program via USB/DFU mode in STM32 Cube Programmer.
Or you have some kind of Arduino or mbed loader on it, and you can deliver firmware via their IDE, or as a drag-n-drop USB MSC Device.
2023-11-02 09:30 AM
I got it. Thanks a lot!