Skip to main content
Md Mubdiul Hasan
Associate III
September 21, 2016
Question

How to control buzzer alarm and device power press key by RTC in LSI mode

  • September 21, 2016
  • 2 replies
  • 1026 views
Posted on September 21, 2016 at 02:43

Hi dear all,

I am using STM32F070RB-T6  to control a buzzer for 10 sec beeps and a power ON press key in my circuit.

How to use RTC, DMA here in LSI mode?

Kindly share code and disscuss it.

Thanks in advance.

    This topic has been closed for replies.

    2 replies

    Nesrine M_O
    Associate
    September 21, 2016
    Posted on September 21, 2016 at 10:54

    Hi hasan.md_mubdiul,

    I suggest you to have a look to the RTC example under the STM32F0 cube firmware package:

    STM32Cube_FW_F0_V1.6.0\Projects\STM32F070RB-Nucleo\Examples\RTC\RTC_Alarm

    This example guides you through the different configuration steps by mean of HAL API to ensure Alarm configuration and generation using the RTC peripheral.

    -Syrine-

    Md Mubdiul Hasan
    Associate III
    September 22, 2016
    Posted on September 22, 2016 at 10:05

    Dear Sir,

    I went through this project file.

    My application is different(may be for my ignorance).

    At the beggining I am trying to press a power button, at the same 2 pin will be turn on alternatively, then buzzer and  7segment will reset.

    I need to understand state machine, timer implementation, periferal clock distribution and other things.

    Take a look this code,

      void EXTI0_IRQHandler(void)

           {

             if(EXTI_GetITStatus(USER_BUTTON_EXTI_LINE) != RESET)

             else

            (db_count = 16)

                   EXTI->PR = 0x00000200;

                else

                  EXTI_ClearITPendingBit(EXTI_Line9

         

         

         

          void main()

        

          {

      

             do

               {

                 if(PORTC.PC5 == 0)   //If the KEY_SW1 switch is pressed

                 {

                    Delay_ms(100);    //Switch Debounce

                    if(PORTC.PC5 == 0)//If the switch is still pressed

                    {

                    

                    

                           GPIO_ToggleBits ( GPIOB,TRIAC_CON1_Pin);

                           PORTD.PD2 = 1; //LED7 ON

                           LED7Toggle = 4000;  //4 seconds

                           Delay_ms(1000); //1 Second Delay

                           PORTD.PD2 = 0; //LED OFF

                     }

               } else {    

                     PORTC.PC5 == 0; //If the KEY_SW1 switch is pressed

                    

                      /* set led on */

                    GPIO_SetBits( TRIAC_CON2_Pin);

                    PORTD.PD2 = 1; //LED7 ON

                    LED7Toggle = 4000;  //4 seconds

                    Delay_ms(1000); //1 Second Delay

                    PORTD.PD2 = 0; //LED OFF

                                    }

                     

                            }

                         }while(1);

                        }