cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746G_DISCO USB and UART Issue

david2399
Associate II
Posted on September 01, 2016 at 05:34

Hello,

We bought 10 of these boards and want to run USB host and log screen outputs through UART6 to Hyperterminal. When we run the USB host example, things work fine. When we run UART_com_IT standalone, things work fine. When we combine these, everything works exactly the same until we are in stm32f7xx_hal_uart.c, UART_SetConfig and line

tmpreg

=

(

uint32_t

)

huart

->

Init

.

WordLength

|

huart

->

Init

.

Parity

|

huart

->

Init

.

Mode

|

huart

->

Init

.

OverSampling

;

  When stepping through the assmebly code of this, everything is exact until the

STR R3, [R0] instruction, which is supposed to put 0x0c into address 40011400 to set CR1.

In the standalone case, this register is set and everything works in Hyperterminal. Yet in the combined case, nothing gets written when this instruction is written even though R3 has 0x0c in it, and R0 has the right address in it. Is this a bug in the processor, or is there something I might be setting up wrong?

Thanks in advance for any comments

Dave Bassett

#stm
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
slimen
Senior
Posted on September 21, 2016 at 22:01

Hello,

It's helpful to know which firmware version is using ?

Regards