cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect SDMMC with 48-Pin STM32L431CC ?

MechatronikMonkey
Associate II

On this site is stated that the STM32L431CC 48-Pin Package has an SDMMC interface...

https://www.st.com/en/microcontrollers/stm32l431cc.html

But when have a closer look to the HW Manual, the AF functions are only avail at PORT C and PORT D... witch implies that you need an 64-Pin package...

Is it right that I cant use SDMMC interface with the 48-pin package?

And where can find more information / App Notes about the SDMMC interface? Or is it better to use a normal SPI Interface and use SD Card in SPI Mode?

Best regards

Chris

1 REPLY 1

It is a general landing page "The STM32L431xx family offers nine packages from 32 to 100-pin packages."

Also seem to recall pin escape issues in packages with less than 64-pins.

SPI should be viable, although depressingly slow.

Some of the EVAL and DISCO board reference schematics are illustrative of the interface. You want short, same length, connections. The D0..D3 and CMD pins should have 33-47K pull-up resistors at the socket.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..