cancel
Showing results for 
Search instead for 
Did you mean: 

what will be the problems of using Single VDD Pin (48PIN) connect to VDD voltage by keeping other VDD pins open ?

ARUN C
Associate

I'm using STM32f030C8T6 controller 48pin package ,i want to know what are the difference between digital power supply pin and complementary power supply pin . and also need to know that can i use only Digital power supply to VDD voltage for running the IC?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Uwe Bonnes
Chief

It is the end of the world as we know it.

Using parts in a not specified way will lead to problems not specified.

The part doesn't start.

Groups of pin don't work or stop working.

Allowing other pins to float can cause unpredictable start behaviour.

Avoid lazy/sloppy design.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Super User

> and also need to know that can i use only Digital power supply to VDD voltage for running the IC

Not sure what you mean here. Any power supply that can source enough current can be used for VDD.

If you feel a post has answered your question, please click "Accept as Solution".