cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect 2 die NOR FLASH WITH QUADSPI of H7?

JZou.2
Associate II

These is a 1Gb NOR FLASH with 2 die structure(MT25TL01GBBB8ESF-0AAT).

It request 8 IOs so that I connect both BK1 and BK2 of H7 MCU.

0693W000002lcfJQAQ.png

This above connection correct?

1 ACCEPTED SOLUTION

Accepted Solutions

Depend on the dual-die configuration involved. The STM32H747I-DISCO provides connectivity to pin 6 and 13, and foot-prints to place one or two IC

https://www.micron.com/products/nor-flash/serial-nor-flash/part-catalog/mt25tl01gbbb8esf-0aat

0693W000002lenPQAQ.jpg

The series resistors are there to suppress the ringing/reflections on short traces at high rates

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

1 REPLY 1

Depend on the dual-die configuration involved. The STM32H747I-DISCO provides connectivity to pin 6 and 13, and foot-prints to place one or two IC

https://www.micron.com/products/nor-flash/serial-nor-flash/part-catalog/mt25tl01gbbb8esf-0aat

0693W000002lenPQAQ.jpg

The series resistors are there to suppress the ringing/reflections on short traces at high rates

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..