cancel
Showing results for 
Search instead for 
Did you mean: 

How to calibrate the ADCs on STM32F4 using the HAL library? (on the F4 HAL library I do not see any HAL adc calibration functions)

Henry Brasil
Associate II
Posted on January 24, 2018 at 09:33

How to calibrate the ADCs on STM32F4 using the HAL library? (on the F4 HAL library I do not see any HAL adc calibration functions)

may be it does not need calibration?

thanks

1 REPLY 1
Posted on January 24, 2018 at 21:34

There's no ADC calibration in 'F4. Read the ADC chapter of Reference Manual for your chip.

(Question to ST: I was told Cube is there to facilitate portability - wouldn't it then be appropriate to add the requested function, even if dummy?)

JW