2015-05-06 4:03 AM
I want to have a sample of system clock at MCO pin of STM32F107RC micro controller.
I use dspin firmware library for driving stepper motor. The on board crystal is 8MHz and system clock set to be 72MHz. I add this code to ''dspin.c'': GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); and I add the below line code in ''SetSysClockTo72()'' function at ''system_stm32f10x.c'' file. RCC->CFGR &= (uint32_t)0xF6FFFFFF; //HSE clock selected as MCO source But I don't have no clock output on this pin. please guide me thanks yasamin2015-05-06 4:17 AM
RCC->CFGR = (RCC->CFGR & (uint32_t)0xF0FFFFFF) | (uint32_t)0x08000000;
JW2015-05-09 2:24 AM
Hi
I add the below code RCC->CFGR = (RCC->CFGR & (uint32_t)0xF0FFFFFF) | (uint32_t)0x08000000; in ''SetSysClockTo72(void)'' function at ''system_stm32f10x.c''. But I have the same problem yet!!! please guide me to solve my problem. thanks2015-05-09 3:47 AM
MCO pin should be configured in alternate function mode.
2015-05-09 10:14 PM
Hi
I configured MCO pin in alternate function mode by adding this code to ''dspin.c'': GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); is it wrong? and I add the below line code in ''SetSysClockTo72()'' function at ''system_stm32f10x.c'' file. RCC->CFGR = (RCC->CFGR & (uint32_t)0xF0FFFFFF) | (uint32_t)0x08000000; But I don't have no clock output on this pin. yasamin2015-05-10 4:49 AM
Evidently you're doing something wrong, or it would work..
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Output HSE clock on MCO pin ---------------------------------------------*/
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
RCC_MCOConfig(RCC_MCO_HSE);
// RCC_MCOConfig(RCC_MCO_SYSCLK);
// If these work you'll need to check if you have PLL2 configured and running
}
2015-05-11 2:21 AM
2015-05-12 4:25 AM
I am using external interrupts. STM32F407 is not handling interrupt at speed of greater than 2MHz.
/* Includes ------------------------------------------------------------------*/ #include ''stm32f4xx.h'' #include ''stm32f4xx_syscfg.h'' #include ''stm32f4xx_rcc.h'' #include ''stm32f4xx_gpio.h'' #include ''stm32f4xx_exti.h'' #include ''misc.h'' EXTI_InitTypeDef EXTI_InitStructure; void EXTILine0_Config(void); void LEDInit(void); void main(void) { LEDInit(); EXTILine0_Config(); EXTI_GenerateSWInterrupt(EXTI_Line0); while (1) { } } void LEDInit() { GPIO_InitTypeDef GPIO_InitStructure; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE); /* Configure the GPIO_LED pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_Init(GPIOD, &GPIO_InitStructure); } void EXTILine0_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* Enable GPIOA clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* Enable SYSCFG clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); /* Configure PA0 pin as input floating */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Connect EXTI Line0 to PA0 pin */ SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0); /* Configure EXTI Line0 */ EXTI_InitStructure.EXTI_Line = EXTI_Line0; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); /* Enable and set EXTI Line0 Interrupt to the lowest priority */ NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x01; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x01; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); } void EXTI0_IRQHandler(void) { if (((EXTI->PR & EXTI_Line0) != (uint32_t)RESET) && ((EXTI->IMR & EXTI_Line0) != (uint32_t)RESET)) { GPIOD->ODR ^= 0x8000; EXTI->PR = 0x0001; } } Please help me!2015-05-14 6:05 AM
Hi Ahmed,
You have already submitted your question in another thread ( ). Please avoid switching from one topic to another in the same thread. Thanks & Best Regards -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-05-14 7:55 AM
I think he posted here first, as creating a ''New'' thread is far less apparent/obvious than replying to an older one.
Please just delete patently Off-Topic posts, or move them if the forum software permits that.Thanks, -Clive