cancel
Showing results for 
Search instead for 
Did you mean: 

How to add X-CUBE-AWS middleware package in STM cube IDE 1.14.0

Nagarajan
Associate III

I am using STM32H563-ZI nucleo board. I would like to add X-CUBE-AWS extension package with this Microcontroller. Could you please tell the procedure to integrate this with STM cube IDE?

11 REPLIES 11

I have my own external flash memory which has 16MB capacity. I have generated external loader file also for this flash memory with NUCLEO-H563 board. How can i replace the permanent storage backend of the example application to my external flash memory. I am not finding any related information about external flash component of the STM32H573I-DK in the MEMORY section of linker script file in this demo project.

 

Nagarajan_0-1716387540208.png

 

AWS and ARM both are providing secured communication only right?

why do we need both IOTDeviceDefender and mbedTLS?

Can i use any one of the security systems?