2021-04-21 4:24 PM
Now I am using stm32f103c8 and i'd like to write flash directly in launch period
So I did make it write erase and read data using Hal_functions as you can see under
/*
* sjk_flash.c
*
* Created on: 2021. 4. 21.
* Author: sungjinkim
*/
#include "sjk_flash.h"
#define FLASH_SECTOR_MAX (64U)
typedef struct
{
uint32_t addr;
uint16_t length;
}Flashtbl_t;
static Flashtbl_t flash_tble[FLASH_SECTOR_MAX];
static bool FlashInSector(uint16_t sector_number, uint32_t addr, uint32_t length);
bool FlashInit(void)
{
bool ret = true;
for(int i = 0 ; i < FLASH_SECTOR_MAX; i++)
{
flash_tble[i].addr = 0x8000000 + i * 1024;
flash_tble[i].length = 1024;
}
return ret;
}
static bool FlashInSector(uint16_t sector_number, uint32_t addr, uint32_t length)
{
bool ret = false;
uint32_t sector_start;
uint32_t sector_end;
uint32_t flash_start;
uint32_t flash_end;
sector_start = flash_tble[sector_number].addr;
sector_end = flash_tble[sector_number].addr + flash_tble[sector_number].length - 1;
flash_start = addr;
flash_end = addr + length - 1;
if((sector_start >= flash_start) && (sector_start <= flash_end))
{
ret = true;
}
if((sector_end >= flash_start) && (sector_end <= flash_end))
{
ret = true;
}
if((flash_start >= sector_start) && (flash_start <= sector_end))
{
ret = true;
}
if((flash_end >= sector_start) && (flash_end <= sector_end))
{
ret = true;
}
return ret;
}
bool FlashErase(uint32_t addr, uint32_t length)
{
bool ret = false;
FLASH_EraseInitTypeDef init;
HAL_StatusTypeDef status = HAL_ERROR;
uint32_t page_error;
int16_t start_sector_number = -1;
uint32_t sector_count = 0;
for(int i = 0; i < FLASH_SECTOR_MAX; i++)
{
if(FlashInSector(i, addr, length) == true)
{
if(start_sector_number < 0)
{
start_sector_number = i;
}
sector_count++;
}
}
if(sector_count > 0)
{
HAL_FLASH_Unlock();
init.TypeErase = FLASH_TYPEERASE_PAGES;
init.Banks = FLASH_BANK_1;
init.PageAddress = flash_tble[start_sector_number].addr;
init.NbPages = sector_count;
status = HAL_FLASHEx_Erase(&init, &page_error);
HAL_FLASH_Lock();
}
if(status == HAL_OK)
{
ret = true;
}
return ret;
}
bool FlashWrite(uint32_t addr, uint8_t* p_data, uint32_t length)
{
bool ret = true;
HAL_StatusTypeDef status = HAL_OK;
if(addr % 2 != 0)
{
return false;
}
HAL_FLASH_Unlock();
for(int i = 0; i < length; i += 2)
{
uint16_t data = 0;
data |= p_data[i + 0] << 0;
data |= p_data[i + 1] << 8;
status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_HALFWORD, (addr + i), (uint64_t)data);
if(status != HAL_OK)
{
ret = false;
break;
}
}
HAL_FLASH_Lock();
return ret;
}
bool FlashRead(uint32_t addr, uint8_t* p_data, uint32_t length)
{
bool ret = true;
uint8_t* p_byte = (uint8_t*)addr;
for(int i = 0; i < length; i++)
{
p_data[i] = p_byte[i];
}
return ret;
}
But I don't know How many times it would be endure
About 100 series? or 10000 over?
regards
2021-04-21 4:45 PM
JW
2021-04-21 5:02 PM
Thankyou i acted like finger princess..