2018-02-09 5:29 AM
send an receive data from modem
2018-02-09 8:02 AM
Assuming some sort of energy metering project.
What modem specifically are you using? Can you provide links to description or documentation?
Would imagine USART, SPI or I2C would be normative modes of connectivity.
2018-02-13 3:59 AM
'euridis modem ' for remote communication between an energy meter and a concentrator (stm32 ...)
2018-02-13 4:45 AM
A modem - any modem - is simply device which connects a 'host' (or 'DTE') to some communications link.
https://en.wikipedia.org/wiki/Modem
Details of how the modem interacts with its 'host' will be in the modem's documentation.
So: have you studiedthis modem'sdocumentation?
As
Turvey.Clive.002
said, UART/USART, SPI, I2C would be common ways for a modem tointeract with its 'host'. Again, this will be detailed
in the modem's documentation.A common protocol for
a modem to
interact with its 'host' overUART/USART is to use so-called AT Commands:
https://en.wikipedia.org/wiki/Hayes_command_set
And, again,
this will be detailed
in the modem's documentation.2018-02-13 5:02 AM
Are we talking about this:
?And, thus, about this:
https://en.wikipedia.org/wiki/IEC_62056
?But, presumably, not this:
?2018-02-13 5:57 AM
euridis modem is going to be realized by me and I find difficulty in the design part of this modem that will realize the communication between energy meter and PC
2018-02-13 6:03 AM
So are you familiar with the basics of how any modem interacts with its 'host' ?
Surely, that would be the place to start ...