cancel
Showing results for 
Search instead for 
Did you mean: 

How do I set the NUCLEO-L476 to Low power mode

Schuyler
Senior

I need to use the energy collection mode of ST25 to wake up L4. The software used now is En.X-Cub-NFC7. How can I modify the example code to set L4 to low power mode and wake up L4 only through the energy of ST25?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Uwe Bonnes
Chief

You can either hope that HAL/Cube provides what you want or read, study and  understand the reference manual w.r.t. to power saving and eventually code yourself.

Andrew Neil
Super User

See the links from @Piranha here for a discussion of correctly entering & leaving low-power modes:

https://community.st.com/t5/stm32cubeide-mcus/dbgmcu-cr-dbg-stop-setting-ignored/m-p/616354/highlight/true#M22468

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.