2019-12-05 01:42 AM
Dear fellow STM32 users,
I've Managed to get the current consumption on my l100C discovery board down to 3.8µA with only the RTC running on the LSI. Steps that I've performed so far:
What can I do to get the consumption down to the 1.5µA promised in the datasheet? Is it a Software issue or are there leaky capacitors on the discovery board?
Thanks in advance for any hints. :)
2019-12-05 01:49 AM
What happens if you disable PINC8 too?
2019-12-05 02:28 AM
Hi Uwe,
just tried it - no measurable difference in consumption...
2020-03-03 03:01 AM
I managed to achieve around 3.8µA on the STM32L100CDiscovery board in stop mode incl. LSI clock and BOR, but no PVD or DEBUG. Here's how in case someone has a similar issue:
When I originally posted my question, my biggest mistake was to not set PH-0 and PH-1 as analog inputs.