2009-10-05 07:32 AM
How do I change the audio file?
2011-05-17 04:24 AM
Hi,
I've got a question concerning the application note AN2739 (playing audio files with I2S audio codec), using the STM3210E-EVAL board: When I load the application onto the board, the standard STM32-family-presentation appears. Where is this audio file located and how do I change the audio file playing? Sorry, if it's a stupid question, I'm not very experienced. Thank you in advance for your reply! Danny2011-05-17 04:24 AM
DFU PC installation has DFU file manager in its program folder, that can extract and again create the .dfu files. I guess the wav file is added as binary content, so no trouble at all!
2011-05-17 04:24 AM
See page 21 of the AN :-D
It's external NOR in the FSMC iface, preloaded with the presentation data.2011-05-17 04:24 AM
Ok the file (wave)is loaded with the DFU demonstration firmware (STM3210E-EVAL_Demo_NORFlash_V2.0.0.dfu) as bin file.
But how do I change the audio file ? It is a binary file. How can i change a wave file to a binary file ? Or how can I store another wave file as the DFU standard wave file ? greeting Roger [ This message was edited by: roger.schweizer on 28-09-2009 10:32 ]